Skip to main content
mwiesmeier9
Visitor II
August 26, 2015
Question

Workbench limitations

Posted on August 26, 2015 at 09:19

Hi,

i want to run motors with Rs < 0.01 Ohm and Ld<0.010 mH (low voltage high current), but the Motor Control Workbench is limited to this values.

Can someone give me the formula to compute all the parameters from the header files, to do it by myself?

Thanks for your help

Marco

#motor-control-workbench
This topic has been closed for replies.

2 replies

Gigi
ST Employee
September 7, 2015
Posted on September 07, 2015 at 14:36

Ciao Marco

It is an information that we can't deliver in this way.

I suggest to contact you nearest ST sales office.

Ciao

Gigi

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards