Skip to main content
Associate II
August 1, 2024
Question

Why the start of ovm mode is set to these value?

#define OVM_VREF_MODE1_START ((int32_t)29717)
#define OVM_VREF_MODE2_START ((int32_t)31186)

The ratio between these two value is not sqrt(3)/2. What is the voltage unit used in these calculation? Or when a have a Valpha equal to 32767, what is the truth voltage in real world?

 

Thanks.

    This topic has been closed for replies.

    2 replies

    KonechoAuthor
    Associate II
    August 1, 2024

    Also, the document "A priori determination of flux and torque current PI gains" says that the PI module uses a voltage factor of VBusDC/2^16, is this correct?Seems like it should be 3VBusDC/2^16.

    KonechoAuthor
    Associate II
    August 2, 2024

    Found something interesting:

    the PI controller and FF think the voltage reference is Vbus/2,

    the PWMC_SetPhaseVoltagefunction thinks it's Vbus/sqrt(3),

    PWMC_SetPhaseVoltage_OVM thinks it's 2Vbus/3,

    circle limit in OVM mode thinks it's -- 2Vbus/pi, right?