Associate III
August 18, 2025
Question
Why the MCSDK hangs out on the generated board in the STMC board designer
- August 18, 2025
- 5 replies
- 665 views
I used MotorControl Workbench_6.4.1 and used the Board designer to generate the simplest design for the sixStep inverter design.
I choose STM32030K as the MCU and assigned back emf as the speed and position control and also configured the Phase voltage generation and M1 specification and every thing gets a green check mark. then I tried to build a project with the created inverter board file and when I select to generate the project, the MotorControl Workbench Just shows a blank screen and nothing happens. what's going on wrong?
I have attached the inverted json file to the post.