Skip to main content
SAhme.0
Visitor II
May 8, 2019 10:11 AM UTC
Question

Why motor profiler is not running with STM3240G-Eval with STEVAL-IHM028V2?

We have STM3240G-Eval and STEVAL-IHM028V2 boards.

we are trying to run the bldc motor of (24 pole-pairs,1.4KW) with motor profiler (MC-SDK 5.3.3) and we also tried with another motor (8 pole-pairs , 30W) .

the profiler isn't able to calculate Rs, Ls and Ke Values. but after 20% to 25% of profiling it is showing "The measurement is talking too much time".

we also decrease current and max. speed but the result are same.

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
Jun 15, 2021 6:49 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards