Skip to main content
Zt Liu
Senior III
June 25, 2018
Question

Why Motor Profiler doesn't support STEVAL-SPIN3202/3201 boards?

  • June 25, 2018
  • 5 replies
  • 1167 views
Posted on June 25, 2018 at 15:01

Since 

STSPIN32F0/A already contains a F0 core,

and there is st-link on board.

Why motor profiler does not support these two boards?

#spin32f0
This topic has been closed for replies.

5 replies

Diandi Zhu
Associate II
July 10, 2018
Posted on July 10, 2018 at 20:32

I saw a post they say F0 just not powerful enough to run the profiler. Only F3 and up

Zt Liu
Zt LiuAuthor
Senior III
July 11, 2018
Posted on July 11, 2018 at 17:57

Thanks for reply, Diandi!

That's what I think too,

for if you compile the sample project in STSW-SPIN3201, 

the flash and ram are almost 100% utilized!

Diandi Zhu
Associate II
July 11, 2018
Posted on July 11, 2018 at 18:09

I encountered the same problem. At beginning I tried to generate a trueStudio project, compiled with &39-o3&39 optimization on. The code size is less than 32k but it didn&39t(I read a post after pointing out that the hal library for F0 is not supported in TrueStudio yet. I don&39t know if that&39s the problem. And I also tried LL driver with no luck) So I switched to keil(you can get free license for f0), now the compiled code size is about 23k with only hall sensor enabled.

I have a post about code size here:

https://community.st.com/0D50X00009XkW99SAF

 

cedric H
ST Technical Moderator
August 6, 2018

Dear all,

You are right, F0 is not powerful enough to do profiling. The main reason is that there is no FPU which is mandatory.

Regards

Cedric

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards