Skip to main content
Dror Laor
Visitor II
March 30, 2017
Question

Why does my BLDC motor stop during acceleration?

  • March 30, 2017
  • 2 replies
  • 822 views
Posted on March 30, 2017 at 10:12

I'm currently evaluating STSPIN32F0 as a solution for BLDC polygon motor control & drive.

My EVB is STEVAL-SPIN3201.

The application is:

  • 38V nominal
  • 8A max @ acceleration
  • 60 deg displaced hall sensors
  • 2 pole pairs
0690X00000603gyQAA.jpg

My Motor configuration is

0690X00000606f4QAA.png

When probing for hall-sensors feedback I get:

0690X00000606euQAA.png

Sensors 1-3 correspond to channels 1-3 

respectively.

b-emf was also measured:

0690X00000606ezQAA.png0690X00000606cBQAQ.png0690X00000606cLQAQ.png

My sensor configuration is

0690X00000606cQQAQ.png

When measuring b-emf on UVW terminals I get

0690X00000606cRQAQ.png

UVW correspond to channels 1-3 respectively.

When trying to speed ramp to 15,000 in 15,000 ms I get the following UVW drives:

0690X00000606cSQAQ.png

Motor starts spining for approx. 10s and then stops.

MC Workbench displays the flowing data after motor is stopped:

0690X00000606ZgQAI.png

My SystemDriveParams folder & MC Workbench project is attached as a .zip file.

No changes have been made in the source files except commenting out &sharpdefine EXAMPLE_POTENTIOMETER and &sharpdefine FIRMWARE_VERS ''STM32 FOC SDK\0Ver.4.4.2''

Any Ideas?

Thanks,

Dror

#polygon #stspin32f0 #bldc #hall-sensors
This topic has been closed for replies.

2 replies

Enrico Poli
ST Employee
April 7, 2017
Posted on April 07, 2017 at 14:03

Hello Dror,

In your configuration file the PWM frequency is set to 16k and the execution rate is 2, as a consequence the 'bandwidth' of the FOC algorithm is 16k/2 --> 8 kHz. Not so fast.

Moreover you are using a motor with low inductance value, so and high PWM frequency is recommended in order to keep the current under control.

Please, try the attached setup with fPWM = 24k.

________________

Attachments :

SDK43x-STEVAL-SPIN3201-sankyo_hall.stmcx.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyj1&d=%2Fa%2F0X0000000bBZ%2F5ilfsM7LkZMGlUfXoA23IQdteVy6BFkC4BSX0UZl4U0&asPdf=false
Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards