Skip to main content
Associate III
Jul 30, 2025 3:15 PM UTC
Question

Which ST control board should I choose to detect motor parameters?

Hello Everybody,
I have a high-power BLDC motor with a rated power of 200W and a nominal voltage of 24V, resulting in a current draw of approximately 10A. I intend to use Motor Profiler to detect detailed motor parameters (e.g., B-EMF constant). Could you advise on which ST control board is suitable? I know there are many control boards like NUCLEO-G431RB. Given the high current, is the control board with the Three-Shunt current sensing inappropriate? If so, what alternative control board should I select? Thank you!

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
Aug 7, 2025 12:20 PM UTC

Hello @DF_MC,

Opening BOARD in the MCSDK workbench and selecting Power Boards and Inverter Boards, you will be able to make your selection based on electrical characteristics. 
The NUCLEO-G431RB is a versatile board that can meet your requirements.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA