Skip to main content
AShin.5
Associate II
May 16, 2022
Question

Where can i get the firmware of steval-spin3204??

Where can i get the firmware of steval-spin3204?? that is, stsw-spin3204.zip.

I have the steval-spin3204 board for testing a motor.

I try to automatically generate the firmware with X-CUBE-MCSDK-Y tool.

Unfornately, I got the error of "freemarker template error" on mc_tasks.c

And, I suffered from this error of "freemarker template error"

I did not solve this error.

stsw-spin3204.zip is more easy for me.

Thanks in advance.

AShin.

This topic has been closed for replies.

3 replies

AShin.5
AShin.5Author
Associate II
May 16, 2022

I try to automatically generate the firmware with X-CUBE-MCSDK-Y tool.

Unfornately, I got the error of "freemarker template error" on mc_tasks.c

And, I suffered from this error of "freemarker template error"

   

 

/**

  ******************************************************************************

  * @file    mc_tasks.c

  * @author  Motor Control SDK Team, ST Microelectronics

  * @brief   This file implements tasks definition

  *

  ******************************************************************************

  * @attention

  *

  * <h2><center>&copy; Copyright (c) 2019 STMicroelectronics.

  * All rights reserved.</center></h2>

  *

  * This software component is licensed by ST under Ultimate Liberty license

  * SLA0044, the "License"; You may not use this file except in compliance with

  * the License. You may obtain a copy of the License at:

  *                             www.st.com/SLA0044

  *

  ******************************************************************************

  */

/* Includes ------------------------------------------------------------------*/

//cstat -MISRAC2012-Rule-21.1

#include "main.h"

//cstat +MISRAC2012-Rule-21.1

#include "mc_type.h"

#include "mc_math.h"

#include "motorcontrol.h"

#include "regular_conversion_manager.h"

#include "mc_interface.h"

#include "digital_output.h"

#include "pwm_common.h"

#include "mc_tasks.h"

#include "parameters_conversion.h"

#include "mcp_config.h"

/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* USER CODE BEGIN Private define */

/* Private define ------------------------------------------------------------*/

/* Un-Comment this macro define in order to activate the smooth

   braking action on over voltage */

/* #define  MC.SMOOTH_BRAKING_ACTION_ON_OVERVOLTAGE */

  #define CHARGE_BOOT_CAP_MS  ((uint16_t)10)

  #define CHARGE_BOOT_CAP_MS2 ((uint16_t)10)

  #define OFFCALIBRWAIT_MS    ((uint16_t)0)

  #define OFFCALIBRWAIT_MS2   ((uint16_t)0)

  #define STOPPERMANENCY_MS   ((uint16_t)400)

  #define STOPPERMANENCY_MS2  ((uint16_t)400)

  #define CHARGE_BOOT_CAP_TICKS  (uint16_t)((SYS_TICK_FREQUENCY * CHARGE_BOOT_CAP_MS) / ((uint16_t)1000))

  #define CHARGE_BOOT_CAP_TICKS2 (uint16_t)((SYS_TICK_FREQUENCY * CHARGE_BOOT_CAP_MS2)/ ((uint16_t)1000))

  #define OFFCALIBRWAITTICKS     (uint16_t)((SYS_TICK_FREQUENCY * OFFCALIBRWAIT_MS)   / ((uint16_t)1000))

  #define OFFCALIBRWAITTICKS2    (uint16_t)((SYS_TICK_FREQUENCY * OFFCALIBRWAIT_MS2)  / ((uint16_t)1000))

  #define STOPPERMANENCY_TICKS   (uint16_t)((SYS_TICK_FREQUENCY * STOPPERMANENCY_MS)  / ((uint16_t)1000))

  #define STOPPERMANENCY_TICKS2  (uint16_t)((SYS_TICK_FREQUENCY * STOPPERMANENCY_MS2) / ((uint16_t)1000))

/* USER CODE END Private define */

#define VBUS_TEMP_ERR_MASK ~(MC_OVER_VOLT | MC_UNDER_VOLT | MC_OVER_TEMP)

/* Private variables----------------------------------------------------------*/

static FOCVars_t FOCVars[NBR_OF_MOTORS];

static PWMC_Handle_t *pwmcHandle[NBR_OF_MOTORS];

static CircleLimitation_Handle_t *pCLM[NBR_OF_MOTORS];

//cstat !MISRAC2012-Rule-8.9_a

static RampExtMngr_Handle_t *pREMNG[NBR_OF_MOTORS];   /*!< Ramp manager used to modify the Iq ref

                                                    during the start-up switch over.*/

static uint16_t hMFTaskCounterM1 = 0; //cstat !MISRAC2012-Rule-8.9_a

static volatile uint16_t hBootCapDelayCounterM1 = ((uint16_t)0);

static volatile uint16_t hStopPermanencyCounterM1 = ((uint16_t)0);

static volatile uint8_t bMCBootCompleted = ((uint8_t)0);

/* USER CODE BEGIN Private Variables */

/* USER CODE END Private Variables */

/* Private functions ---------------------------------------------------------*/

void TSK_MediumFrequencyTaskM1(void);

void FOC_Clear(uint8_t bMotor);

void FOC_InitAdditionalMethods(uint8_t bMotor);

void FOC_CalcCurrRef(uint8_t bMotor);

void TSK_MF_StopProcessing(  MCI_Handle_t * pHandle, uint8_t motor);

MCI_Handle_t * GetMCI(uint8_t bMotor);

static uint16_t FOC_CurrControllerM1(void);

void TSK_SetChargeBootCapDelayM1(uint16_t hTickCount);

bool TSK_ChargeBootCapDelayHasElapsedM1(void);

void TSK_SetStopPermanencyTimeM1(uint16_t hTickCount);

bool TSK_StopPermanencyTimeHasElapsedM1(void);

void TSK_SafetyTask_PWMOFF(uint8_t motor);

/* USER CODE BEGIN Private Functions */

/* USER CODE END Private Functions */

/**

  * @brief  It initializes the whole MC core according to user defined

  *         parameters.

  * @param  pMCIList pointer to the vector of MCInterface objects that will be

  *         created and initialized. The vector must have length equal to the

  *         number of motor drives.

  * @retval None

  */

__weak void MCboot( MCI_Handle_t* pMCIList[NBR_OF_MOTORS] )

{

  /* USER CODE BEGIN MCboot 0 */

  /* USER CODE END MCboot 0 */

 

  if (MC_NULL == pMCIList)

  {

    /* Nothing to do */

  }

  else

  {

   

    bMCBootCompleted = (uint8_t )0;

    pCLM[M1] = &CircleLimitationM1;

 

    /**********************************************************/

    /*    PWM and current sensing component initialization    */

    /**********************************************************/

    pwmcHandle[M1] = &PWM_Handle_M1._Super;

    FreeMarker template error (DEBUG mode; use RETHROW in production!):

The following has evaluated to null or missing:

==> PWM_Init  [in template "mc_tasks.c.ftl" at line 765, column 7]

----

Tip: If the failing expression is known to legally refer to something that's sometimes null or missing, either specify a default value like myOptionalVar!myDefault, or use <#if myOptionalVar??>when-present<#else>when-missing</#if>. (These only cover the last step of the expression; to cover the whole expression, use parenthesis: (myOptionalVar.foo)!myDefault, (myOptionalVar.foo)??

----

----

FTL stack trace ("~" means nesting-related):

  - Failed at: ${PWM_Init}  [in template "mc_tasks.c.ftl" at line 765, column 5]

----

Java stack trace (for programmers):

----

freemarker.core.InvalidReferenceException: [... Exception message was already printed; see it above ...]

  at freemarker.core.InvalidReferenceException.getInstance(InvalidReferenceException.java:134)

  at freemarker.core.EvalUtil.coerceModelToTextualCommon(EvalUtil.java:481)

  at freemarker.core.EvalUtil.coerceModelToStringOrMarkup(EvalUtil.java:401)

  at freemarker.core.EvalUtil.coerceModelToStringOrMarkup(EvalUtil.java:370)

  at freemarker.core.DollarVariable.calculateInterpolatedStringOrMarkup(DollarVariable.java:100)

  at freemarker.core.DollarVariable.accept(DollarVariable.java:63)

  at freemarker.core.Environment.visit(Environment.java:334)

  at freemarker.core.Environment.visit(Environment.java:340)

  at freemarker.core.Environment.visit(Environment.java:340)

  at freemarker.core.Environment.process(Environment.java:313)

  at freemarker.template.Template.process(Template.java:383)

  at com.st.microxplorer.codegenerator.CodeEngine.freemarkerDo(CodeEngine.java:333)

  at com.st.microxplorer.codegenerator.CodeEngine.genCode(CodeEngine.java:245)

  at com.st.microxplorer.codegenerator.CodeGenerator.generateOutputCode(CodeGenerator.java:5062)

  at com.st.microxplorer.codegenerator.CodeGenerator.generateSpecificCode(CodeGenerator.java:4367)

kelvin.wang
Associate II
May 23, 2022

steval-spin3204 support 6step only. If you want to generate code by MCSDK, you can only use the example code listed below the MCSDK.

AShin.5
AShin.5Author
Associate II
May 23, 2022

Many Thanks, Mr. kelvin ****.