Skip to main content
DTort.1
Associate III
August 29, 2021
Solved

Where are the pins for measuring back emf when configured in the Motor SDK?

Hello, I am using a B-G431B-ESC1 board and want to set up my motor with speed control via back emf in MotorControl Workbench 5.4.7 or 5.Y.2 (I checked both there and there). On the board, these are pins PA4, PC4, PB11 and PB5, but I don't see this initialized in the SDK. In the speed sensing section, I have sensor-less (Observer + PLL) installed.

This topic has been closed for replies.
cedric H
cedric HBest answer
ST Technical Moderator
August 30, 2021

Hello,

The MC SDK is dedicated to FOC algo. Our FOC algo does not use back emf sensing, this is why the back emf pins are not initialized.

As the board is also 6steps compatible, everything is ready to do speed control via back emf sensing, but this configuration is not developed yet.

Regards

Cedric

3 replies

Tesla DeLorean
Guru
August 29, 2021
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
cedric H
cedric HBest answer
ST Technical Moderator
August 30, 2021

Hello,

The MC SDK is dedicated to FOC algo. Our FOC algo does not use back emf sensing, this is why the back emf pins are not initialized.

As the board is also 6steps compatible, everything is ready to do speed control via back emf sensing, but this configuration is not developed yet.

Regards

Cedric

DTort.1
DTort.1Author
Associate III
August 30, 2021

Thanks a lot! I understood everything, I just did not take into account that back emf is not used with FOC.

If 6-step control comes up it would be great.