Skip to main content
just4u78
Associate II
Dec 10, 2024 1:16 AM UTC
Solved

When will the Motor Control Software Pack for CubeMX be possible?

I want to create a project with the Motor Control library using CubeMX.

 

However, The Motor Control library is not registered as a software package in CubeMX, Now.

 

Refering some application note, it says to use CubeMX's X-CUBE-MCSDK, but this software package is not available in CubeMX.

 

I wonder if the X-CUBE-MCSDK software package will be available again in the future.

This topic has been closed for replies.
Gael A
Gael ABest answer
ST Employee
Dec 10, 2024 10:04 AM UTC

Hello just4u78,

You are right, the MCSDK is not available as a CubeMX package. This may be subject to discussion in the future but there is currently no plan to make it part of it. You can still use the MCSDK as a standalone tool, that calls CubeMx whenever generation is needed.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

2 replies

Gael A
Gael ABest answer
ST Employee
Dec 10, 2024 10:04 AM UTC

Hello just4u78,

You are right, the MCSDK is not available as a CubeMX package. This may be subject to discussion in the future but there is currently no plan to make it part of it. You can still use the MCSDK as a standalone tool, that calls CubeMx whenever generation is needed.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.
just4u78
just4u78Author
Associate II
Dec 10, 2024 10:26 AM UTC

I don't understand why this library was excluded from the software pack.

 

In the current situation, if I want to create a new MCU board with the MC library, I must either create a new board in MCWorkbench board manager tool and use it, or configure the project manually.

 

I want to create an MCU board that can only give commands like Motor Pilot.

(You called it a Performer Device in Motor Control Protocol Suite Manual)

 

I want to say that "It's not easy for a beginner to set it up through the Board Manager".