Skip to main content
WSega.1
Associate II
March 21, 2022
Question

When will ST Motor Profiler support EVSPIN32G4?

The EVSPIN32G4 is not an option when you 'select hardware' in the latest version of the Motor Profiler (5.Y.4). Will it be supported in an upcoming release? Also, is there any plan to support higher RPM profiling? The limit is 16kRPM right now.

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
August 30, 2023

Dear WSega,

Firstly, we would like to sincerely apologize for the delay in replying to your post.
If your point is still pertinent, on future 6.2 release, you will be able to use it for profiling feature.
On current versions, the displayed 16K RPM max speed it is only an example, you can set an higher value.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA