Skip to main content
jartim
Associate III
April 14, 2023
Question

When the motor profiler is used - 1: do the L and R values apply to a single phase coil, or are they values measured across two driver outputs, i.e. two phase coils in series? 2: Are they DC measurements or measured at the PWM frequency?

..

This topic has been closed for replies.

1 reply

Gael A
ST Employee
April 17, 2023

Hello @jartim​,

Concerning your first question, R value is measured across two driver outputs, and then is divided by 2 before getting returned to Motor Profiler. L value is calculated using R value previously determined and measured Rise Time. Both values are averaged from a sum incremented at each PWM frequency loop for a definite number of times.

I hope this answers your question well.

Best Regards,

Gaël A.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.