Skip to main content
Vladislav.Sedlak
Visitor II
January 11, 2022
Question

What is the best practice to setup unknown escooter motor (800W) parameters to fit STSPIN32G4? Without load motor works perfect. But under load, when I try the torque mode, the motor is too weak on the beginning.

  • January 11, 2022
  • 1 reply
  • 619 views

I'm using MotorControl Workbench 5.Y.3 + Keil MDK

Testing on EVSPIN32G4 and custom STSPIN32G4

54V battery, 16A nom current

This topic has been closed for replies.

1 reply

DTort.1
Associate III
January 12, 2022

Perhaps your question is related to my question. And I have the same problem.

I think about the fact that the FOC algorithm cannot correctly start the rotation of the motor under a heavy load and this requires trapezoidal control at the first moment. I would be just as interested to know ST's answer.

https://community.st.com/s/question/0D53W00001J9V06SAF/is-it-possible-to-start-the-motor-under-heavy-load-in-foc-mode