Skip to main content
MMa.1893
Associate III
Feb 26, 2020 3:08 AM UTC
Solved

what does "auxiliary sensor" mean?

MCSDK 5.4.3

i use hall as main feedback sensor, but i noticed that i can also choose sensor-less as auxiliary sensor. what does this mean?

This topic has been closed for replies.
Mathieu Casties
Mathieu CastiesBest answer
Visitor II
Mar 11, 2020 12:50 PM UTC

​Right you can only use one or the other under normal situation.

4 replies

Mathieu Casties
Visitor II
Feb 27, 2020 2:18 PM UTC

​Hello, if you choose sensor-less as auxiliary sensor, it means that both the hall observer and  the sensor-less observer will be generated and will run in parallel .

Both will determine the angle and speed but only the Hall observer will be used to drive the motor. 

This feature add CPU workload and is mainly used for debug purpose.

Onorm.1
Associate II
Jul 8, 2021 12:07 PM UTC

Hello mathieu, I don't really understand why the option of auxiliary sensor is selectable if it's just for debugging purpose. To me having an auxiliary sensor can add to redundancy in case of main sensor failure. I am surprised that aux sensor feature is only there for debugging knowing that you can greatly increase reliability of your product with the possilbity to switch on sensorless ( for example ) when your main sensor fails...

MMa.1893
MMa.1893Author
Associate III
Feb 28, 2020 4:01 AM UTC

ok, so no benifits on sensor-less auxiliary sensor under normal situation, right?

Mathieu Casties
Mathieu CastiesBest answer
Visitor II
Mar 11, 2020 12:50 PM UTC

​Right you can only use one or the other under normal situation.