Skip to main content
Associate
Apr 2, 2025 10:58 AM UTC
Question

Vertical Take off in STEVAL FCU001

Hi All,

I am beginner to drones. We assembled one drone using STEVAL FCU. 002. board ,  recommended set. of motors and. propellers along with battery. 

We Chose different. frame.  than. one recommended . It is smaller in size. 

While flying , vertical take. off. could. not be achieved.

Can someone guide please ?

Motor connections , Clock wise. ,  anti clock wise in reference. to alignment. of. the boards are checked. already.

It is ST board. so. come equipped with all driver , frimware etc.

Thanks in advance.

Early and accurate response is. appreciated.

Regards,

 

30 replies

mmdave1Author
Associate
Apr 2, 2025 11:02 AM UTC

Please find video. to. understand the behaviour of drone.

Peter BENSCH
ST Technical Moderator
Apr 2, 2025 12:34 PM UTC

Welcome @mmdave1, to the community!

You can't see much on your video (start of the motors at 0:2.366 > 0:2.399), but it looks like the propellers are not mounted correctly.

  • What is their direction of rotation?
  • Can you please show a photo from above where you can see the tilt of the propeller blades?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mmdave1Author
Associate
Apr 2, 2025 3:24 PM UTC

Hi Peter,

 

Thanks. for prompt. revert.

We have cross checked with ST documentation and it is in line.

Sharing one photo , Motors. and propellers are aligned. in that way.

Regards,

mmdave1_0-1743607460643.png

 

Peter BENSCH
ST Technical Moderator
Apr 2, 2025 3:34 PM UTC

The direction of rotation is correct, but which propeller with which tilt did you use where?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Apr 2, 2025 1:18 PM UTC

@mmdave1 wrote:

While flying , vertical take. off. could. not be achieved.


This doesn't make sense: you have to take off before you can be flying!

Do you mean that you didn't achieve enough lift with the motors?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mmdave1Author
Associate
Apr 2, 2025 3:26 PM UTC

Hi Andrew,

 

That is the issue.

It does. not. take off. properly and does not achieve the lift. though motors and everry other. parts are as recommended. by ST , except frame.

Andrew Neil
Super User
Apr 2, 2025 3:33 PM UTC

@mmdave1 wrote:

everry other. parts are as recommended. by ST , except frame.


As beginners, perhaps it would be better to start with the actual frame, motors, and propellers provided in the kit by ST?

STEVAL-DRONE02: https://www.st.com/en/evaluation-tools/steval-drone02.html

 

AndrewNeil_2-1743607911121.png

That way you know for sure that everything is correct & compatible

 

BTW: What's. with. all. the. full. stops. in. your. posts?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
KnarfB
Super User
Apr 2, 2025 1:23 PM UTC

STEVAL-FCU001V2 is F4, not F0.

What firmware?

The stock firmware basically used to work. 

Form the video it looks like a wiring / coordinate system issue.

hth

KnarfB 

mmdave1Author
Associate
Apr 2, 2025 3:29 PM UTC

@ KnarfB,

 

Standard ST firmware STSW-FCU001 . It has come. preloaded with STEVAL FCU00V1.

 

mmdave1_1-1743607740198.png

 

Explorer
Apr 22, 2025 3:05 PM UTC

hello i have exactly the same problem.

mmdave1Author
Associate
Apr 24, 2025 6:00 AM UTC

Hi Rania1,

Please let  us  know if  you achieve any progress.

Similarly , we will  also let you know.

Regards,

NovaPoseidon
Associate
Apr 24, 2025 11:03 AM UTC

We also have the same problem.

We are making a FCU based on STEVAL-FCU001V2 as a study project. We originally ordered the STVEAL-FCU001V2 via digikey from this link: "https://www.digikey.in/en/products/detail/stmicroelectronics/STEVAL-FCU001V2/22522577", 3D printed the STDRONE002 frame and ordered the 8520 motors and 65mm propellers from this link: "https://robu.in/product/65mm-blade-propeller-prop-8520-cw-ccw-coreless-brushed-motor-indoor-racing-drone-quad-copter/". We are using the exact battery that ST recommended "3.7v 600mAh and 25C discharge rating" purchased from this link: "https://robu.in/product/bonka-3-7v-600mah-25c-1s-lithium-polymer-battery-pack/". But to no extent did it even took off. And in the rare cases that our drone took off, it spined rapidly in the yaw axis.

Any help would be appreciated.

Associate
Mar 25, 2026 1:07 PM UTC

Hi, I'm in the same situation. I bought the official drone kit and FCU board as a school study project for a custom flight controller stabilization code. The hardware is as follows:

- steval-FCU001V2 board
- steval-drone02 drone kit

I used the UM3117 https://www.st.com/resource/en/user_manual/um3117-how-to-build-your-own-minidrone-with-the-stevaldrone02-and-stevalfcu001v2-stmicroelectronics.pdf  manual as a reference. Compared to the materials and manuals available for version V1 of the drone kit and the steval fcu001V1, this V2 resources and manuals seems less comprehensive to me, and some of the connection diagrams aren’t very clear. Some resources for V1 will certainly still be valid for V2, but this isn't guaranteed, and in that case it would have been better to include them in the official documentation for V2.

 

My main issues now are as follows: I can’t get it to fly with the factory-loaded firmware, and I can’t even flash a new firmware or erase prev flash contents.

1) When I connected the motors according to the manual, I found that the motors with white and black wires (I believe the ones that are supposed to rotate CCW) are reversed compared to the manual; if wired as per the manual, the propellers push air upward instead of downward… so I inserted the motor connectors with the white and black wires reversed from what was indicated. (I saw a correction sheet mentioning something like this, but only for a specific batch of version V1 years ago; nothing for v2)

2) The board already had the factory firmware, and with that I couldn’t get it to take off or stay stable in flight with ST_BLE_DRONE app; it only rises about 2 cm, spins in place, or sometimes accidentally hovers at a height of 2 cm but spins wildly in yaw, making circles, and then crashes into something (with initial calibration done and battery fully charged)

I downloaded the reference firmware from the STM website, “STSW-FCU001 Reference Design Firmware for Mini Drones,” at the link https://www.st.com/en/embedded-software/stsw-fcu001.html

This appears to be the firmware on the device, as when I connect a UART-USB adapter to the FCU’s P7 connector and view the serial terminal, I see printf debug output that exactly matches the version and date in the printf code line in main.c

Thinking it might be a PID or parameter issue, I connected an H7 Nucleo board to use solely as an STLink and debugger via STM32CubeProgrammer (after I removed the nucleo MCU power supply and reset jumpers). The programmer connects successfully and correctly detects the FCU’s STM32F401 MCU target, but when attempting to read the flash to save an existing program, it reads all 0x00000. Furthermore, upon checking, it appears that the control bytes are incorrect, enabling a flash read/write protection that shouldn’t be present.
Furthermore, when manually setting the read protection to “disabled” and clicking “Apply,” the programmer freezes and the program stops responding, so I can’t even modify those settings… I can’t even perform a full flash erase; the sector erase always fails.

This makes me suspect that the option bytes might be corrupted in the default firmware that was loaded, or that they have been modified in some way I can’t explain—simply connecting a programmer doesn’t alter them on its own. At this point, I’m not sure how to recover the device if they cannot be reset or modified through the programmer. This could potentially mean the MCU is effectively locked, and the only workaround might be replacing it with a fresh, non-compromised one—which is obviously not ideal.

 

I have a few questions:

  1. Were you able to successfully import the project into the STM32 Cube IDE? I was able to, but only using a version prior to 2.xxx. Furthermore, if I open the IOC settings, the project no longer compiles; the middleware folders get altered, and if you try to add a peripheral or change any settings in the IOC, the project and necessary includes get corrupted, and a large number of compilation errors are generated…
  2. Also, regarding the reference FW, I don’t understand which modules or folders are auto-generated by the IDE used by the FW developer, or if it’s custom code imported or copied from another project and manually adapted without auto-generated drivers.
  3. Is there a proper procedure for correctly importing the reference project and being able to modify IOC settings without corrupting it?
  4. Has anyone managed to get it flying with the default firmware, or can anyone provide their wiring diagrams or modifications made to the firmware and hardware so I can program it and get it flying properly?

It’s a bit of a shame because it’s a beautiful kit with everything you need, open fw and hw, but getting it up and running seems very laborious… especially if there are already these initial issues.
And I've seen several discussions about this kit with similar issues, but it's unclear whether they've been resolved or not. I'd like to figure out if it's a problem affecting only a few people, if it's just me.