Skip to main content
omid hamdi
Associate III
Sep 2, 2019 12:27 AM UTC
Solved

Vector control ac motor sensorless

with stm32g431 how can detect motor parameter in ac induction motor without motor profiler only with algorithm program in side micro controller without computer software

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:46 PM UTC

Dear @omid hamdi​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

2 replies

Laurent Ca...
Senior III
Jun 28, 2021 4:51 AM UTC

Adding of STM32 Motor Control topic.

Best regards.

Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:46 PM UTC

Dear @omid hamdi​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards