Solved
Varied Practical RPM with STEVAL-IPM10B and NUCLEO-F302R8 in ST Motor Control Workbench
- 4 replies
- 2291 views
I am currently facing an issue with the RPM readings while running a motor using the STEVAL-IPM10B and NUCLEO-F302R8 in conjunction with the ST Motor Control Workbench.
Upon measurement with a tachometer, I observed a difference between the practical RPM values and the readings displayed on the dashboard. Even though I utilized the Motor Profiler to generate motor parameters.
I had attached the Program files for your reference.
Thanks in Advance.