Skip to main content
ABouv.1
Visitor II
January 22, 2020
Question

Using the Motor Control Workbench Monitor on custom board

Hello,

I am using a custom board and I would like to use the Motor Control Benchs Custom Monitor.

As far as I understand I have to activate serical communication and simply generate and flash my custom board.

My problem is that I can not connect to my custom board. I thought that this might be the case because I only use an ST-Link to connect to my board (so just 4 cables).

Can someone help me out? What am I doing wrong? Do I have to connect something different to the ST-Link adapter?

This topic has been closed for replies.

2 replies

Laurent Ca...
Senior III
September 11, 2020

Dear ABouv.1

Do you have still this problem to solve?

Best regards

Laurent Ca...

Laurent Ca...
Senior III
September 23, 2020

Dear @ABouv.1​ 

I guess you don't have to solve this problem anymore, therefore I consider this post closed.

If not, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...