Skip to main content
Explorer
August 28, 2023
Solved

using stm32wl55ccu to drive 3 phase bldc

Hi ,

I am using stm32wl55ccu 48 pin QFN MCU to drive a 3 phase brushless motor using 3-phase complementary PWM output signals using TIMER 1. I have seen at the datasheet that this 48 QFN package is missing the complementary output of TIMER1 ,Channel 3, TIM1_CH3N (which is present at the BGA version). Is it possible to generate the 3-rd phase complementary output PWM signal in another way ?(like using timer 2 in a master/slave configuration).

Thank you, Joe.

    This topic has been closed for replies.
    DBE
    DBEBest answer
    ST Employee
    September 7, 2023

    Hello YY55,

    It is technically possible to synchronize TIM1(master) and TIM2(slave), examples are available in the reference manual of the chip (chapter 24.3.26 and 25.3.19):

    https://www.st.com/resource/en/reference_manual/rm0434-multiprotocol-wireless-32bit-mcu-armbased-cortexm4-with-fpu-bluetooth-lowenergy-and-802154-radio-solution-stmicroelectronics.pdf

    But your firmware will have to take care about the deadtime insertion between the high side and low side on the third phase (which will be done automatically on phase 1 and 2 by TIM1 in your case).

    Another solution could be to choose (if possible), a gate driver that needs only 3 PWM input signals ( like L6230: https://www.st.com/en/motor-drivers/l6230.html ) 

    Best regards

     

     

    If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

    1 reply

    DBE
    DBEBest answer
    ST Employee
    September 7, 2023

    Hello YY55,

    It is technically possible to synchronize TIM1(master) and TIM2(slave), examples are available in the reference manual of the chip (chapter 24.3.26 and 25.3.19):

    https://www.st.com/resource/en/reference_manual/rm0434-multiprotocol-wireless-32bit-mcu-armbased-cortexm4-with-fpu-bluetooth-lowenergy-and-802154-radio-solution-stmicroelectronics.pdf

    But your firmware will have to take care about the deadtime insertion between the high side and low side on the third phase (which will be done automatically on phase 1 and 2 by TIM1 in your case).

    Another solution could be to choose (if possible), a gate driver that needs only 3 PWM input signals ( like L6230: https://www.st.com/en/motor-drivers/l6230.html ) 

    Best regards

     

     

    If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.