Skip to main content
Associate III
March 21, 2025
Question

User settings being cleared by code generation by Workbench.

  • March 21, 2025
  • 2 replies
  • 726 views

Hello Everybody,

MCSDK:6.3.0

CubeMX: 6.1.1

Workbench : 6.3.0

CubeIDE : 1.15.0

 

When using Workbench to regenerate the FOC code, the additional peripheral settings I configured in CubeMX, such as IO, Timer, and ADC, are all cleared. As a result, I have to manually reconfigure them every time. Could you please provide a solution to avoid this issue? Thank you.

I remember that in earlier versions of Workbench (v5.4.x), there was an "Update CubeMX" button after generating the code. Pressing this button would preserve the additional peripheral settings. Could you please advise where to enable this feature in the current version?

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
March 21, 2025

@Vincent7 wrote:

additional peripheral settings I configured in CubeMX, such as IO, Timer, and ADC, are all cleared. ?


Are you taking care to keep all your user code within the /* USER CODE xxx */  markers?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Vincent7Author
Associate III
March 21, 2025

Hello Andrew Neil,

Thank you for your reply.

Yes, I wrote everything inside the /* USER CODE xxx */ markers.
The strange thing is, all the code is still there.
But after generating code from Workbench and then clicking "Run CubeMX",
when the CubeMX window pops up, I can see that all my IO/ADC/Timer configurations are gone.