Skip to main content
Daniel Husztikd
Associate II
July 14, 2017
Question

USART not working in Motor Control Library

Posted on July 14, 2017 at 15:32

I am using the Motor Control Library, to control a BLDC motor with Hall sensors. I would like to use the uart for my own purposes. If I enable uart, it dumps trash (since it tries to communicate with the MC workbench) if I disable it, even if I configure it normally, it do not work. What do you suggest? Removing the MC Workbench communication part, or disabling the usart in the control_stage_parameters, and reconfigure again? 

Thanks!

Daniel

#foc #motor-control-workbench #stspin32f0 #motor
This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards