Associate III
Feb 16, 2025 8:19 PM UTC
Solved
Updating motor mechanical parameters : Inertia and friction
- 1 reply
- 1063 views
I am trying to control a 24V PMSM type motor using ST Motor Control Workbench version 6.3.1 with the FOC.
I have run Motor Profiler and then gotten the electrical and mechanical parameters.
I have three questions and can anybody help/answer them?
- I am running Motor Profiler without load? Am I doing correct?
- When creating a project using Motor Control Workbench, do I need to update the inertia and friction coefficients in the motor stage depending on the load (please see attachment)? If the answer is no, where should I include the inertia and friction of the load in the project?
- May I measure PMSM type motor inertia and friction coefficients with load? If yes, how can I do it?
Thanks in advance.