Skip to main content
Associate
Oct 15, 2025 4:24 PM UTC
Solved

"unknown protocol c" Java Exception when generating project in MC workbench

Hi,

I'm in charge of the motor driver for a new project we've started working on. I freshly installed MotorControl Workbench, CubeMX and the IDE. After setting all parameters in Workbench and hitting "Generate the project" button I get a Java runtime Exception "unkown protocol c". I've hit a wall trying to fix this as there's almost no info about similar issues on the web.
I tried uninstalling and installing different versions, too.

Using windows 11 pro, 24H2.

 

Any suggestions what might go wrong here? I've tried installing the oracle JDK and using that instead of the openJDK runtime but I couldn't get Workbench to use it (this was the only info I could find).
Thanks for any help on this!

nb_coresightBest answer
Associate
Nov 13, 2025 10:46 AM UTC

So I noticed that some other tools have issues too. Could it be the é ("special character") in the windows username (and subsequently in the home-directory path name) that causes issues with scripts and such? 
Trying with IT to remove it but this will take some time. Any suggestions welcome

12 replies

GMA
ST Technical Moderator
Oct 16, 2025 6:30 AM UTC

Hello @nb_coresight,

If the code generation proceeds to the main.c file, you can use the generated project.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Associate
Oct 16, 2025 6:49 AM UTC

Thank you,

Unfortunately, it doesn't even reach that point. It fails right away, pretty much.

GMA
ST Technical Moderator
Oct 16, 2025 7:17 AM UTC

Hello @nb_coresight,

You can try using MCSDK6.4.1 available here.

Refer to the STM32Cube environment chapter of the MCSDK6.3.0 release note (accessible through Workbench tool > About > Documentations) for the STM32CubeMX version (v6.11.0 is expected) and firmware packages to be used.

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Associate
Oct 30, 2025 4:00 PM UTC

Anyone else with any suggestions?
Still stuck on this. It HAS to be something my machine, but I have no idea what could cause this.

ST Employee
Nov 3, 2025 10:47 AM UTC

Hi @nb_coresight ,

 

this issue has been identified and should be fixed within next release of STM32CubeMx 6.16.0 which will be available in the coming weeks.

Nevertheless, can you please check with the version 6.14.0 and let us know your status.

 

Thanks in advance

Regards

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
Associate
Nov 4, 2025 10:19 AM UTC

Thank you.
I will try as soon as I have the time to.

Associate
Nov 6, 2025 2:34 PM UTC

Nope, still the same issue 

 

nb_coresight_0-1762439646030.png

 

nb_coresightAuthorBest answer
Associate
Nov 13, 2025 10:46 AM UTC

So I noticed that some other tools have issues too. Could it be the é ("special character") in the windows username (and subsequently in the home-directory path name) that causes issues with scripts and such? 
Trying with IT to remove it but this will take some time. Any suggestions welcome

GMA
ST Technical Moderator
Nov 27, 2025 4:17 PM UTC

Hello @nb_coresight,

The STM32CubeMX 6.16 tool is available here.
As you mentioned, try selecting a path without special characters.

GMA_0-1764259928229.png

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Associate
Feb 16, 2026 5:10 PM UTC

Just to follow up here: we eventually changed the username removing "special" characters (é in my case) in the home-directory path, this did the trick.

GMA
ST Technical Moderator
Feb 17, 2026 7:20 AM UTC

Hello @nb_coresight,

Thank you for your feedback.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA