Skip to main content
Associate
Jun 20, 2025 5:48 PM UTC
Question

Unable to Read Data from L6470

 Using HAL_SPI_TransmitReceive properly. I've corrected the code to send the command 0x25 followed by two dummy bytes (0x00, 0x00) in a single transaction to read the ACC register.

However, now I’m facing a new issue: no matter what value I set for ACC, when I read it back, I always get 0x80 0x00 0x89 (i.e., 128 0 137). I double-checked the write sequence as well and it appears to complete successfully.(I am able to execute run command)

Dev29_0-1750441274571.png

 

I’ve also attached the image and my updated code for reference. Any suggestions on what I might be missing?

Additionally, I’ve already set all KVALs and MAX_SPEED to their maximum values, yet the motor won't go beyond ~1000 steps/sec. Beyond that, it starts vibrating heavily and doesn’t rotate at all, I am using NEMA 17 and NEMA 23 with 24v Supply and tried with no load condition and with some load as well. Phase resistance for NEMA 17 is 3.3R  and Inductance 2.8 mH/phase and fot NEMA 23 has 2.23R and Inductance: 2.25 mH plus it is heating even just pasing 1A to 55 C.

I've attached an image and included my updated code for reference. Any suggestions on what I might be missing would be greatly appreciated.

Thanks again for your help and patience!

void L6470_SendCommand(uint8_t *cmd, uint8_t len)
{

 for (uint8_t i = 0; i < len; i++) {
 	L6470_CS_Low();
 HAL_SPI_Transmit(&hspi2, &cmd[i], 1, HAL_MAX_DELAY);
 L6470_CS_High();
 }

 HAL_Delay(1); // small delay for stability
}

void L6470_Run(uint8_t dir, float speed)
{

 uint32_t spd =speed;
 uint8_t cmd[] = {
 (dir == 0) ? 0x50 : 0x51, // RUN forward/reverse
 (uint8_t)(spd >> 16) & 0xFF,
 (uint8_t)(spd >> 8) & 0xFF,
 (uint8_t)(spd & 0xFF)
 };
 L6470_SendCommand(cmd, 4);
}
void L6470_SetACC(){

	uint8_t ACC_cmd[] = {
	0x05, // ACC register address (Write command)
	 (0x25 >> 8) & 0xFF, // MSB = 0
	 (0x25 & 0xFF) // LSB = 0x8A = 138
	};

	 L6470_SendCommand(ACC_cmd, 3);
}
void L6470_SetDCC(){
	uint8_t DCC_cmd[] = {
	0x05, // ACC register address (Write command)
	 (0x08A >> 8) & 0xFF, // MSB = 0
	 (0x08A & 0xFF) // LSB = 0x8A = 138
	};

	 L6470_SendCommand(DCC_cmd, 3);
}

void L6470_SetABS_POS(){
	uint8_t ABS_cmd[] = {
		0x01,
		 (0x00 >> 16) & 0x3F,
		 (0x00 >> 8) & 0xFF,
			(0x00 & 0xFF)

		};

		 L6470_SendCommand(ABS_cmd, 4);
}

void L6470_SET_MAX_SPEED(){
	uint8_t MAX_SPEED_cmd[] = {
			0x07,
			(0x3CFA >> 8) & 0xFF, // MSB = 0
		 (0x3CFA & 0xFF) // LSB = 0x8A = 138
			};

			 L6470_SendCommand(MAX_SPEED_cmd, 3);
}
void L6470_SET_MIN_SPEED(){
	uint8_t MIN_SPEED_cmd[] = {
			0x08,
			(0x00 >> 8) & 0xFF, // MSB = 0
		 (0x00 & 0xFF) // LSB = 0x8A = 138
			};

			 L6470_SendCommand(MIN_SPEED_cmd, 3);
}
void L6470_SET_FS_SPD(){
	uint8_t FS_SPD_cmd[] = {
				0x15,
				(0x3ff >> 8) & 0xFF, // MSB = 0
			 (0x3ff & 0xFF) // LSB = 0x8A = 138
				};

				 L6470_SendCommand(FS_SPD_cmd, 3);
}
void L6470_KVALs(){
	 uint8_t kval_max = 0xFF;

	 uint8_t kval_hold_cmd[] = { 0x09, kval_max };
	 L6470_SendCommand(kval_hold_cmd, 2);

	 uint8_t kval_run_cmd[] = { 0x0A, kval_max };
	 L6470_SendCommand(kval_run_cmd, 2);

	 uint8_t kval_acc_cmd[] = { 0x0B, kval_max };
	 L6470_SendCommand(kval_acc_cmd, 2);

	 uint8_t kval_dec_cmd[] = { 0x0C, kval_max };
	 L6470_SendCommand(kval_dec_cmd, 2);
}
void L6470_SET_STEP_MODE(){
	uint8_t step_mode_cmd[] = {
	 0x16, // STEP_MODE register address
	 0x00 // Set to full step
	};
	L6470_SendCommand(step_mode_cmd, 2);
}
void L6470_SET_OCD_TH (){
	uint8_t ocd_cmd[] = { 0x13, 0x0F }; // 0x0F = max threshold
	L6470_SendCommand(ocd_cmd, 2);
}
void L6470_SET_STALL_TH(){
	uint8_t stall_cmd[] = { 0x14, 0x7F }; // Max sensitivity
	L6470_SendCommand(stall_cmd, 2);
}
void L6470_INT_SPEED(){
	uint16_t int_speed_val = (uint16_t)(930 * 16.77);
	uint8_t int_speed_cmd[] = {
	 0x0D, // INT_SPEED register
	 (uint8_t)(int_speed_val >> 8), // MSB
	 (uint8_t)(int_speed_val & 0xFF) // LSB
	};
	L6470_SendCommand(int_speed_cmd, 3);
}
uint32_t L6470_ReadABS_POS(void) {
 static uint8_t receivedData[3] = {0x00,0x00, 0x00};
	uint8_t tx_buf[3] = {0x25, 0x00, 0x00}; // 0x25 = GET_PARAM | ACC (0x05), followed by 2 dummy bytes

	L6470_CS_Low();
//	 HAL_Delay(10);
	 HAL_SPI_TransmitReceive(&hspi2,tx_buf,receivedData,3,HAL_MAX_DELAY);
	 L6470_CS_High();
	 //HAL_Delay(10);
 printf("receivedData[0] %d \r\n",receivedData[0]);
 printf("receivedData[1] %d \r\n",receivedData[1]);
 printf("receivedData[2] %d \r\n",receivedData[2]);


}
void L6470_Init()
{
	L6470_SetACC();
		L6470_SetDCC();
		L6470_SetABS_POS();
		L6470_SET_MAX_SPEED();
		L6470_SET_MIN_SPEED();
		L6470_SET_FS_SPD();
		L6470_KVALs();
		L6470_SET_STEP_MODE();
		L6470_SET_OCD_TH();
		L6470_SET_STALL_TH();
 L6470_INT_SPEED();
}
int main(void)
{
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 MX_SPI2_Init();
 /* USER CODE BEGIN 2 */
 L6470_Init();
 L6470_Run(0, 33554); // RUN forward at max speed 500step/sec
 L6470_ReadABS_POS();
 while (1)
 {
 }
}

 

This topic has been closed for replies.

1 reply

Cristiana SCARAMEL
ST Employee
Jul 24, 2025 2:11 PM UTC

Hello @Dev29 ,

have you verified that the CPHA/CPOL configuration is consistent with that required by the device?
Is the device in HiZ status? Otherwise the writing of some registers is rejected.

Regarding the rotation problem: I suggest you read the application notes dedicated to Voltage mode: 
AN4144 - Voltage mode control operation and parameter optimization

You can find a detailed description on how to optimize the parameters.

"If you feel a post has answered your question, please click ""Accept as Solution"""