Skip to main content
Associate
Nov 19, 2024 3:06 PM UTC
Solved

Troubleshooting of STEVAL-IHM028V2

Hello,

While I did tests with my motor control STEVAL-IHM028V2, I made a mistake to schort-circuit the three-phase output ! Then, I smelled a burning smell and no voltage is given in the three-phase output . When I checked the bottom face of the device, I noticed that some resistors (R74, R75 and R69) are burned (see attached images). Also, the W7 and W8 jumpers are short-cicuited. How could I fix this issue ?

N.B. The schematic of the STEVAL-IHM028V2 is attached.

Cordially

Tarek

 

This topic has been closed for replies.
GMA
GMABest answer
ST Technical Moderator
Nov 27, 2024 8:20 AM UTC

Hello @Tarek_ben,

You can try to replace all of these components (resistors/jumper).
Set a conservative limitation current on your external DC supply.
Verify that DC voltages are correctly generated on the board. 
Monitor the current consumption when relaunching test.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

5 replies

Tarek_benAuthor
Associate
Nov 21, 2024 12:42 PM UTC

Any answer about this ?

GMA
ST Technical Moderator
Nov 26, 2024 3:51 PM UTC

Hello @Tarek_ben,

On your IHM028V2.jpg picture, nothing seems to be burned... 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Tarek_benAuthor
Associate
Nov 26, 2024 4:02 PM UTC

Thank you for the answer.

If you zoom in on the resistances R74, R75 and R69, you can see a black line in the middle of these resistances.