Skip to main content
Associate III
Apr 2, 2025 10:29 AM UTC
Solved

TRIG_X Signal with the STEVAL-PTOOL4A

Hello,

I am reading the documentation of the STEVAL-PTOOL4A, I have noticed that it is equipped with a TRIG_X  to enable/disable the DC/DC booster. I don't know if I understood well its functionality, but It will mainly turn on/off all the board including the MCU. So each time, we trigger, the MCU will execute from the reset_handler right? But maybe I want to keep the MCU on always, and I want to scan an input and when it is On, it will turn on or off the motor depending on its status. How it could be done by TRIG_X? Or I should use in this case another GPIO and I configure it manually? For example could I use the one of the potentiometer instead?

 

Thank you

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 2, 2025 1:04 PM UTC

It's like a power button if R82 is removed. Otherwise it doesn't do anything.

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Peter BENSCH
ST Technical Moderator
Apr 2, 2025 12:57 PM UTC

In the original state of the STEVAL-PTOOL4A (R82 is fitted), U5 (L6981, incidentally not a booster but a buck regulator) is permanently switched on and TRIG_X has no effect because EN_BUCK is connected to VBATT+.

The DC_DC latch can only work if you remove R82 because EN_BUCK is then controlled by TRIG_X via Q7. When SW1 is pressed or TRIG_X = Low, EN_BUCK is activated, which switches on the buck regulator and thus the entire board. The function of the latch is also described in UM3374, section 5.5.9.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AnthonyKAuthor
Associate III
Apr 2, 2025 12:59 PM UTC

Hello Peter,

Yes that's what I have understood also. It is like a power button. 

 

Thank you for your help.

 

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 2, 2025 1:04 PM UTC

It's like a power button if R82 is removed. Otherwise it doesn't do anything.

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.