Question
Timers
Hi,
So I presently have this problem. As seen in the picture, my timer1 time base is set to 1919 and it has a 48MHz clock source, which means I should produce signals with frequency of 25kHz. But this is not the case. instead the output signals from the timer is about 1.2kHz.
What could possibly be wrong? How is it possible that the timebase is set to 1919 for a 48MHz clock source and it doesnt produce the right 25kHz frequency?