Skip to main content
AndrewSibiryack
Associate III
April 16, 2022
Solved

There is such a document: "AN5464-Position control of a three-phase permanent magnet motor using X‑CUBE‑MCSDK or X‑CUBE‑MCSDK-FULL"

Hi!

There is such a document: "AN5464-Position control of a three-phase permanent magnet motor using X‑CUBE‑MCSDK or X‑CUBE‑MCSDK-FULL"

It describes the method of setting the PID controller. It is necessary to reset all coefficients and gradually increasing the P-component to achieve its fluctuations. Question: before that, do you need to set the motor to the zero position or another angle? or how did the CUBE generate and compile?

Thank you in advance for your help!

P.S.It is not possible to configure the PID controller. The best thing that happened is shaking in the set positions and the engine is very warm!

This topic has been closed for replies.
AndrewSibiryack
AndrewSibiryackBest answer
Associate III
April 16, 2022

It is not possible to configure the PID controller. The best thing that happened is shaking in the set positions and the engine is very warm!

1 reply

AndrewSibiryack
AndrewSibiryackAuthorBest answer
Associate III
April 16, 2022

It is not possible to configure the PID controller. The best thing that happened is shaking in the set positions and the engine is very warm!