Skip to main content
Vdsfg.1
Visitor II
Jul 16, 2020 1:04 AM UTC
Solved

The latest version of the FOC SDK does not support ACIM motors. Which version does it need to support PFC and ACIM motors?

..

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:36 PM UTC

Dear @PBoni.1304​ and @Vdsfg.1​ 

There is now in the last SDK version a demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

4 replies

Claire O.
ST Employee
Jul 20, 2020 9:19 AM UTC

dear Vdsfg.1,

I am sorry, we have not such library so far... It's part of our roadmap but not before 2021.

Thanks,

Claire

PBoni.1304
Visitor II
Mar 24, 2021 8:34 PM UTC

News about ACIM Motors support for "FOC SDK"?

Laurent Ca...
Senior III
Jun 15, 2021 7:38 AM UTC

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK). 

Best regards

Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:36 PM UTC

Dear @PBoni.1304​ and @Vdsfg.1​ 

There is now in the last SDK version a demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards