Skip to main content
Visitor II
October 20, 2024
Question

Support for MCSDK for STM32H747XIH6

We have an application where we need to use the STM32H747XI with it's MIPI DSI display and the corresponding application running on CM7 and we need to commutate a BLDC motor on with the CM4. There is support for NUCLEOH745ZI on on the STM32CubeMX but we need to implement it on the STM32H747XI. I tried to port the whole middleware of MotorControl to it but I'm unable to complete my requirement. Is there anyway of acquiring native support for STM32H747I-DISCO for the MCSDK, I have little experience with the STM32 environment.

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
October 20, 2024

Hello @Pirdain_B and welcome to the ST Community.

For Now, as you said the only supported MCU of the STM32H7 Family is the STM32H745ZITx (throw the NUCLEO-H745ZI). For your case, i suggest you to take a working project based on this supported MCU and try to adapt it to your MCU.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.