Skip to main content
Michael Schmid
Associate II
August 16, 2024
Question

STSPIN32G4 for VFD open loop motor speed control

Dear experts,

 

we like to develop new VFD spindle motor controller, with V/Hz open loop control. I am searching for a modern reference design for 220V applications, based on the STSPIN32G4. But I could only find designed for BLDC, focused on FOC, but not V/Hz control. The STSPIN32G4 seem to have everything in 1 chip, including 600V MOSFET driver, except the power stage. So it would just be matter of the Firmware to output a 3 phase variable sine. 

 

Is there a application note or reference design, maybe also for the STSPIN32F0, for a V/Hz motor control? Is there support for CubeMX for this? Inverter motor designs are mentioned many times, just not together with V/Hz. There are older designs from NXP and TI for exactly that, but I want to use the highly integrated STSPIN, also because we are familiar with the STM32 series.

 

Thank you.

This topic has been closed for replies.