Skip to main content
Ritul Shah
Associate II
Feb 16, 2022 12:00 PM UTC
Question

STSPIN32F0: Why does BLDC Motor stop with a Speed Feedback Fault on Loading it?

Hello All,

I am using STSPIN32F0 controller to run a BLDC motor at 1400 RPM. I am using ST Motor Control Workbench and IAR IDE for my project.

Motor Design Specs:

Rated Voltage: 36V

Rated Current: 10Amp

Rated RPM: 1400 RPM

  1. My Motor Starts without any issues
  2. Till the Motor is loaded up to 2 Amps, it works perfectly well
  3. If More than 2 Amp is loaded, the Motor fails to RUN and a SPEED FEEDBACK ERROR or OVER VOLTAGE ERROR is generated.

What can be the problem?

Need your support as soon as possible.

Thank you

Ritul Shah

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
Mar 2, 2022 9:23 AM UTC

Hello,

Please, have a look to ST wiki FAQ page, chapter 2.10.

Frequently Asked Questions (FAQ) - stm32mcu

Best regards.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA