Skip to main content
james farrant
Associate II
May 28, 2025 3:13 PM UTC
Question

STM32G4B1C3

Hello,

I am trying to get my STM32G4B1C3 ESC working for a brushless rc hobbyist motor with unknown motor parameters. I flashed a generic set of parameters to the device and enabled the motor profiler before flashing so that I could estimate them online. 

 

When I connect to the motor pilot app Everything is detected fine with no faults, but then I click begin profiler and it seems to just stall with a high pitch noise and never gets past 7% complete. I have tried swapping the 3 phases in all combinations with no change in behavior:

 

Motor details:

Aerosky MC2212-980KV 

7 pole pairs with standard surface magnets (outboard)

 

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
May 28, 2025 3:21 PM UTC

Hello @james farrant,

The A2212 motor is available from MCSDK6.3.1 delivery.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA