Skip to main content
omid hamdi
Associate III
Aug 15, 2019 10:36 AM UTC
Solved

Stm32g474 and ac motor control

Hi

any one can help to me how can start with stm32 with ac induction motor with library st

need some example is possible use motor workbench v5 for setup induction?

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:47 PM UTC

Dear @omid hamdi​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

3 replies

Laurent Ca...
Senior III
Jun 22, 2021 8:13 AM UTC

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:47 PM UTC

Dear @omid hamdi​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

omid hamdi
Associate III
Jul 9, 2021 4:25 PM UTC

thanks for help resolved