Skip to main content
Mathan Raja
Associate III
Mar 26, 2026 1:38 PM UTC
Solved

STM32G0 MCSDK: Using RCM for extra ADC channel – correct approach?

Hi,

I am using STM32G0 with STM32 Motor Control SDK. ADC1 is used for motor current sensing (triggered by TIM1 for FOC control).

Since STM32G0 has only one ADC and does not support injected channels, I needed to read an additional NTC sensor (ADC channel 8) for motor stator temperature.

I implemented this using Regular Conversion Manager (RCM):

  • Registered ADC channel using RCM_RegisterRegConv()

  • Requested conversion periodically (~300 ms)

  • Read the value after conversion completion

The motor is running stable, and I am able to get temperature readings without visible disturbance.

My question:
Is this a correct and recommended approach for reading an additional analog signal in STM32G0 + MCSDK?

Are there any potential risks (timing issues, FOC accuracy impact) when using RCM alongside motor control?

Or is there a better recommended method for this use case (e.g., external ADC, different MCU, or MCSDK-specific approach)?

Thank you.

GMA
GMABest answer
ST Technical Moderator
Mar 30, 2026 4:13 PM UTC

Hello @Mathan Raja,

This is the correct method according to the comment feature description available in the regular_conversion_manager.c file.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

1 reply

GMA
GMABest answer
ST Technical Moderator
Mar 30, 2026 4:13 PM UTC

Hello @Mathan Raja,

This is the correct method according to the comment feature description available in the regular_conversion_manager.c file.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA