Skip to main content
barisC
Associate
February 10, 2023
Solved

STM32F407 - Servo Motor (SG90) is not work. (PWM output and motor seem to be working properly)

Hello, I am trying to learn bare metal programming and servo motor control with my stm32f407g-disc1 card.

I cannot move the servo motor with stm. I tried with arduino to check if the problem is in the motor and the motor worked. I thought my PWM signal was wrong and I found codes from the internet but it didn't work again. 

I am attaching the code and logic analyzer graphs. Can you help me what could be the problem?

void GPIO_Init(void);
void TIM2_Init(void);
void TIM4_ms_Delay(uint32_t delay);
 
void GPIO_Init(){
	RCC->AHB1ENR |= 1; //Enable GPIOA clock
	GPIOA->AFR[0] |= 0x00100000; // Select the PA5 pin in alternate function mode
	GPIOA->MODER |= 0x00000800; //Set the PA5 pin alternate function
}
 
void TIM2_Init(){
	RCC->APB1ENR |=1;
	TIM2->PSC = 16-1; //Setting the clock frequency to 1MHz.
	TIM2->ARR = 20000; // Total period of the timer
	TIM2->CNT = 0;
	TIM2->CCMR1 = 0x0060; //PWM mode for the timer
	TIM2->CCER |= 1; //Enable channel 1 as output
	TIM2->CCR1 = 500; // Pulse width for PWM
}
 
void TIM4_ms_Delay(uint32_t delay){
	RCC->APB1ENR |= 1<<2; //Start the clock for the timer peripheral
	TIM4->PSC = 16000-1; //Setting the clock frequency to 1kHz.
	TIM4->ARR = (delay); // Total period of the timer
	TIM4->CNT = 0;
	TIM4->CR1 |= 1; //Start the Timer
	while(!(TIM4->SR & TIM_SR_UIF)){} //Polling the update interrupt flag
	TIM4->SR &= ~(0x0001); //Reset the update interrupt flag
}
 
int main(){
	RCC->CFGR |= 0<<10; // set APB1 = 16 MHz
	GPIO_Init();
	TIM2_Init();
	TIM2->CR1 |= 1;
	while(1){
 
		if(TIM2->CCR1 < 2500){
			TIM2->CCR1 = TIM2->CCR1 + 50;
			TIM4_ms_Delay(50);
		}
		else{
			TIM2->CCR1 = 500;
			TIM4_ms_Delay(50);
		}
	}
}

0693W00000YARugQAH.png0693W00000YARuWQAX.png 

Edit: I tried with HAL library but nothings change. Is it possible my STM is broken?

For HAL library, I follow this videos instruction: https://www.youtube.com/watch?v=owbuhblItBA

This topic has been closed for replies.
barisC
barisCBest answer
Associate
February 11, 2023

Okay, after researching the problems for two days, I bought a new servo motor of the same model. And code is working with new motor. I still have no idea why the old motor does not work with stm32.

I didn't see anything about closing the topic, but if any mod sees this message, you can close the topic.

3 replies

Javier1
Principal
February 10, 2023

what about the logic level?

Is your arduino 5v and your stm 3v3?

hit me up in https://www.linkedin.com/in/javiermuñoz/
barisC
barisCAuthor
Associate
February 10, 2023

Yes, arduino gives 5v and stm32 gives 3v3 output voltage.That sounds like it could be a problem, but I didn't see anyone except me using the same card and the same motor and having problems. Am I missing something?

barisC
barisCAuthorBest answer
Associate
February 11, 2023

Okay, after researching the problems for two days, I bought a new servo motor of the same model. And code is working with new motor. I still have no idea why the old motor does not work with stm32.

I didn't see anything about closing the topic, but if any mod sees this message, you can close the topic.