Skip to main content
ASilv.8
Visitor II
September 17, 2019
Question

STM32F303CB Motor control setup can't avoid stalling

Hi,

I am using the STEVAL-ESC001V1 development kit board with a BlueRobotics T200 motor. The motor runs well with the provided SDK firmware and the motor profiler values, but we are having a couple of issues when changing speeds:

  1. The range of the potentiometer maxes out at about 50% turn on either forward or reverse. My PWM range is 1000-2000 and 1500 is "0" since it has forward/reverse.
  2. When we switch the motor from forward to reverse (and vice-versa) after going at full-speed for a few seconds, the motor stalls. It makes a whinding "whoop" sound. Could this be addressed by Rev-up by FOC? What settings can I change to fix this?

Thanks in advance.

This topic has been closed for replies.

3 replies

N_1
Associate III
January 6, 2020

Hello ASliv.8,

I am dealing with the same problem for like a month now. Do you have any solution?

Thank you in advance!

Laurent Ca...
Senior III
September 10, 2020

Dear ASilv.8, dear N

Do you have still this problem to solve?

Best regards

Laurent Ca...

Laurent Ca...
Senior III
September 17, 2020

Dear ASilv.8, dear N

OK. I consider this post closed. Do not hesitate to answer if it is not.

Best regards

Laurent Ca...