Skip to main content
ericc
Associate II
January 6, 2012
Question

STM32 FOC PMSM SDK OverCurrent Protection.

Posted on January 06, 2012 at 05:55

 I wanted to verify that when my HW over current circuit asserts the over-current signal that the effect on the software is the same as an ESTOP.

Or does this input act like a chopper and only terminate the PWM signal for the cycles that the signal is asserted?

Thanks,

Eric
This topic has been closed for replies.

2 replies

Gigi
ST Employee
January 9, 2012
Posted on January 09, 2012 at 09:11

The STM32 FOC PMSM SDK OverCurrent protection acts like an emergency stop. In particular it is performed exploiting the feature of the PWM timer that disables (putting in a predefined state) the six outputs. These signals are kept disabled until the user send another start motor command (after the faut acknowledge).

Regards

Gigi

Laurent Ca...
Senior III
June 21, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards