Skip to main content
11235813
Associate II
July 25, 2022
Question

STM power up with motor running

STM32F405

MCSDK = V5.4.5

f_pwm = 10kHz

High frequency task = 10kHz

Medium frequency task = 1kHz

Position and speed = Hall (main) & STO+PLL (auxiliary)

Current sensing = 3 x 3mOhm shunts

Is it possible with the MCSDK to power up the processor with the motor shaft already rotating and start the controller without the motor coming to a halt? When I try this the motor drives with a very strange noise until the motor is first stopped, after that it runs normally.

I think the cause of this is that the Hall effect initialisation doesn't work correctly if the motor shaft is rotating (perhaps HALL_Clear()->HALL_init_electrical_angle() relies on the motor not rotating?).

Can anyone tell me if this is the likely cause and if so, is there any way to startup the MCSDK code and run the speed/current controller if the motor shaft is already rotating at power up?

This topic has been closed for replies.

1 reply

11235813
11235813Author
Associate II
July 27, 2022

From hall_speed_pos_fdbk.c:

/**

* @brief Clear software FIFO where are "pushed" latest speed information

*     This function must be called before starting the motor to initialize

*     the speed measurement process.

* @param pHandle: handler of the current instance of the hall_speed_pos_fdbk component*

* @retval none

*/

__weak void HALL_Clear( HALL_Handle_t * pHandle )

Does this mean that the motor can't be free spinning when HALL_Clear() is called? By "free spinning" I mean not driven by the STM32 but by something else, for example, a flywheel.