STEVAL-STSPIN3201 Switch off both high and low side MOSFET simultaneously
Hi,
I am trying to implement simple six step motor control using the STEVAL-STSPIN3201 board. However in order to do this I need to be able to switch off both the high and low side MOSFETS in one of the three phases U,V or W. For example for the first commutation I need HSU to be on, LSV to be on while HSW and LSW need to be off, so that only the coils from U to V conduct. However I am running into a problem where I can't switch off both HSW and LSW simultaneously, the outputs from these pins are always complementary. I have tried configuring them as GPIO pins, with pulldown set to low and I still can't get for example HSW & LSW, HSV & LSV, HSU & LSU low simultaneously. Any help to achieve this is appreciated.