Skip to main content
yanjae huh
Visitor II
December 28, 2017
Question

STEVAL-SPIN3202 is Not included in the ST Motor Profiler

Posted on December 28, 2017 at 01:58

Good morning!

I bought Steval-Spin3202, but there is no choice in the SDK for this board.

Is this board not supported by the current version of the SDK?

What are some ways I can try this board?

This topic has been closed for replies.

2 replies

Enrico Poli
ST Employee
January 4, 2018
Posted on January 04, 2018 at 14:14

Hi,

the board is not included into the list of the MC workbenchboards.

However you can set the parameter in order to obtain a compatible project (attached)

________________

Attachments :

SDK43x-STEVAL-SPIN3202-BullRunning.stmcx.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyBP&d=%2Fa%2F0X0000000b4m%2F_O3am0cwXNnLk.yhMQg6tlUsTnGpSLoY0dTBA05sOkM&asPdf=false
Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards