Skip to main content
EShaw.1
Associate III
May 18, 2022 1:09 PM UTC
Solved

STEVAL-SPIN3202. Got it turning. Now need a guidance on where / what file and how I can control the speed.

Hi All,

Got it turning. Now need a guidance on where / what file and how I can control the speed. 

SDK 5.4.8.

6S_STEVAL3202_SL_VM example.

Monitor connects well.

I can start the motor.

Final ramp speed does not work. The only use - setting the direction of rotation.

Measured speed raises from 0 to 4000rpm and motor stops with Fault over "Start-up failure". Motor power indicator jumps to max and stays there.

My application is simple. I need an open loop control. 2 speeds forward, 2 speeds reverse. Stop. Preferably hardware control -3 pin. The only feedback - hardware Fault output.

Questions are:

  1. Where (what settings) can be an error.
  2. Where can I find the code where I can control the speed.
  3. How I can control the speed (what variables are responsible for speed and acceleration?). I assume that it can be done in main.c in while(1) loop.
  4. Could you please direct me to some manual or documentation on 6S_STEVAL3202_SL_VM package.

Thanks in advance for your answers.

Regards,

Edward.

This topic has been closed for replies.
ADAVE.1
ADAVE.1Best answer
ST Employee
May 25, 2022 8:05 AM UTC

Hi Edward,

the errors raised are related to FOC functions that should not be there in the six-step project. You are likely missing something in the generation process.

I suggest to clean the folder and recreate the project from scratch starting from loading the example from 5.Y.4 as follows:

1- in the 5.Y.4 click on the example you are interested in

0693W00000Nqd6OQAR.png 2- After reading, close the readme.txt file and the warning message

3- Click on "Save As" and save the project without renaming it

0693W00000Nqd6xQAB.png4- Click on project generation icon, select the toolchain and click UPDATE

0693W00000Nqd7lQAB.png5- generation process should start with the proper library version (5.Y.4-Full)

0693W00000Nqd8FQAR.png6- Load the project in your development environment and open the file stm32f0xx_mc_it.c where you have to replace the function like in my previous post

0693W00000Nqd9DQAR.png7- build and download the project to the board (or launch the debug mode...)

0693W00000NqdA6QAJ.png8- Open the Motor Pilot, load the defaultApp_6STEP and connect with Speed 115200

0693W00000NqdApQAJ.png 

Regards

Alessio

19 replies

ADAVE.1
ST Employee
May 19, 2022 3:21 PM UTC

Hi Edward,

can you please confirm that you are using MCSDK 5.4.8? This release doesn't include the example you mentioned while MCSDK 5.Y.4 does.

Could you explain which motor are you using and whether you changed any setting or default configuration parameter ?

Regards

Alessio

EShaw.1
EShaw.1Author
Associate III
May 21, 2022 4:29 AM UTC

Hi Alessio,

Thanks for the response.

I am using MCSDK_v5.4.8.

MCSDK 5.Y.4 does not work with STEVAL-SPIN3202. One of your colleagues suggested not to use MCSDK 5.Y.4 but MCSDK_v5.4.8 instead.

0693W00000NqOekQAF.pngThe name of the project - I just changed generic name to 6S_STEVAL3202_SL_VM. Sorry for confusion.

This project was created by ST Motor control Workbench:

File\New Project

Motor B28 - small brushless sensorless inrunner.

Changes to settings:

1) Motor Parameters

2) Overcurrent protection disabled (Tick on main screen and in Analog and input protection) (As I was unable to get it working with protection activated)

3) Speed setting - Sensorless (Oserver+PLL)

4) PWM Freq changed to 12000Hz

5) Control mode- Speed control

Could you please suggest another way of using some example for STEVAL-SPIN3202?

Regards,

Edward.

0693W00000NqOkxQAF.png 

0693W00000NqOfEQAV.png

ADAVE.1
ST Employee
May 23, 2022 7:38 AM UTC

Hi Edward,

it's not clear to me why you have been suggested to use 5.4.8 and if you created the project from scratch (like I see from the image above) or you just load the example of the STEVAL-SPIN3204 (that is compatible with STEVAL-SPIN3202).

Please be aware that if you create a project from scratch in 5.4.8 you are generating a FOC project.

On the other hand, if you load the example you are not able to customize it from the main interface but you have to look for the configuration parameters inside the generated code.

Since SDK 6.0 doesn't currently support F0, I would recommend to use 5.Y.4 and load the example "Six-Step Sensorless and Voltage Mode on a STEVAL-SPIN3202+Shinano LA052-080". Save it WITHOUT renaming the project and generate the code by clicking the UPDATE button. In order to customize the parameters and where to find them into the code, I suggest you to read carefully the attached doc.

Regards

Alessio

EShaw.1
EShaw.1Author
Associate III
May 24, 2022 12:26 PM UTC

Hi Alessio,

Thank you again.

The reason why your colleague suggested that STEVAL-SPIN3202 does not work with 5.Y.4 is that after uploading the project, It is impossible to connect to it with Motor Pilot:

0693W00000NqZ5qQAF.pngThat is why he suggested using 5.4.8 instead.

If you could suggest how to fix connection issue, it would be great.

I'll download the example of the STEVAL-SPIN3204 in 5.4.8 as you suggested and will keep you posted:).

Regards,

Edward.

ADAVE.1
ST Employee
May 24, 2022 12:35 PM UTC

Hi Edward,

Please read section 4.1 of the document I attached in my previous post.

You need to select the proper "qml" file in the MotorPilot installation folder.

Regards

Alessio

EShaw.1
EShaw.1Author
Associate III
May 24, 2022 1:37 PM UTC

After downloading the example of the STEVAL-SPIN3204 in 5.4.8 

This error pops out. May be board STEVAL-SPIN3202 is not that compatible with STEVAL-SPIN3204?

What and where can be tweaked?

0693W00000NqZQPQA3.png

ADAVE.1
ST Employee
May 24, 2022 1:42 PM UTC

Like I wrote in my previous post, I recommend to use 5.Y.4

EShaw.1
EShaw.1Author
Associate III
May 24, 2022 2:02 PM UTC

0693W00000NqZYTQA3.png

EShaw.1
EShaw.1Author
Associate III
May 24, 2022 2:04 PM UTC

same result. 5.Y.4. Correct GUI. No connection. Not on 115200 nor on 9600 Baud

ADAVE.1
ST Employee
May 24, 2022 2:39 PM UTC

Hi Edward,

please try replacing the function "void SysTick_Handler(void)" in the file "stm32f0xx_mc_it.c" with the following lines of code:

void SysTick_Handler(void)
{
 
#ifdef MC_HAL_IS_USED
static uint8_t SystickDividerCounter = SYSTICK_DIVIDER;
 /* USER CODE BEGIN SysTick_IRQn 0 */
 
 /* USER CODE END SysTick_IRQn 0 */
 if (SystickDividerCounter == SYSTICK_DIVIDER)
 {
 HAL_IncTick();
 HAL_SYSTICK_IRQHandler();
 SystickDividerCounter = 0;
 }
 else
 {
 /* Nothing to do */
 }
 SystickDividerCounter ++;
#endif /* MC_HAL_IS_USED */
 
 /* Buffer is ready by the HW layer to be processed */
 if (LL_DMA_IsActiveFlag_TC (DMA_RX_A, DMACH_RX_A))
 {
 LL_DMA_ClearFlag_TC (DMA_RX_A, DMACH_RX_A);
 ASPEP_HWDataReceivedIT(&aspepOverUartA);
 }
 else
 {
 /* Nothing to do */
 }
 
 /* USER CODE BEGIN SysTick_IRQn 1 */
 /* USER CODE END SysTick_IRQn 1 */
 Motor_Device1.uw_tick_cnt++;
 MC_RunMotorControlTasks();
 
 /* USER CODE BEGIN SysTick_IRQn 2 */
 /* USER CODE END SysTick_IRQn 2 */
}

I remind you to save the project without renaming it and generate the code by clicking the UPDATE button in the project generation window of the MCSDK .

Hope this solve your issue in the 5.Y.4 release.

Regards

Alessio