Skip to main content
MM1
Associate II
June 17, 2021
Question

STEVAL-SPIN3202: FOC Duration fault

Hi,

I am trying to spin a BLDC with the STEVAL-SPIN3202.

I get to the point where i can communicate with the board via the ST Motor Pilot and execute commands. However everytime click the Start Button i get the FOC duration fault. Sometimes the Motor spins for a 1/16 turn or so.

Reducing the FOC execution rate did not help.

I am using the workflow with:

Motor Control Workbench 5.Y.1

STM32CubeMX

STM32CubeIDE

I hoe someone can help me

regards Marcus

This topic has been closed for replies.

4 replies

MM1
MM1Author
Associate II
June 28, 2021

no one got an idea what might be wrong?

msingh
Senior
July 6, 2021

Decrease the PWM frequency and that should help. (it worked for me)

MM1
MM1Author
Associate II
July 6, 2021

thanks for your answer, but I already tried that and it did't help :\

msingh
Senior
July 6, 2021

Try changing the PID values then (try reduing Kp or increasing kd or both). If you are using incremental encoders then the try lowering the input Capture filter duration from the MCWB. Good luck!