Skip to main content
FMaur.1
Visitor II
September 7, 2021
Question

STEVAL-SPIN3201: Why does the motor always move in full speed when I want to do sensored control, even if I program different target speeds?

Hello,

I am using the STEVAL-SPIN3201 to drive a motor with sensored FOC.

Inside the code, I use the syntax of the FOC library to program how the motor should move.

I created the project in mc workbench (find the project file attached).

Then I imported it into STM32 IDE and added the following code section inside the main file (user code 3):

 MC_ProgramSpeedRampMotor1(1000/6,0);

     MC_StartMotor1();

     HAL_Delay(8000);

     MC_StopMotor1();

     HAL_Delay(500);

  MC_ProgramSpeedRampMotor1(-100/6,0);

    MC_StartMotor1();

    HAL_Delay(7000);

    MC_StopMotor1();

    HAL_Delay(400);

 /* USER CODE END 3 */

When I test the program, the motor moves first to one direction for 8 seconds, then to the other direction for 7 seconds (as it should do). However, the speed is always the same (according to the motor pilot about 1300 rpm).

Do you know why I can´t program the speed of the motor?

Best regards

Florian Maurer

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
September 15, 2021

Dear @FMaur.1​ 

There is no file attached.

Best regards