Skip to main content
georgeeipi
Visitor II
June 5, 2022
Question

STEVAL-SPIN3201 ST Motor Control Workbench 5.Y.4 Generation failed

  • June 5, 2022
  • 1 reply
  • 839 views

Attempting to load the STEVAL-SPIN3201 example from MCWorkbench 5.Y.4 and attempting to generate the code for the board doesn't work. Attempting to build the resulting project from STM32CubeIDE doesn't work. So I'm guessing that's because the generation didn't work. I'm wondering if the SPIN3201 is at it's EOL? And should I go with some other hardware instead? Or is this problem fixable?

This topic has been closed for replies.

1 reply

ST Employee
December 6, 2022

Dear Customer,

I tried to generate with your configuration but everything seems to work fine.

0693W00000WKMrZQAX.pngI suggest you to install manually the latest firmware with ST CubeMx ( F0 1.11.3) .

To do this, start the CubeMx ,click on the right button "software install or remove the embedded software" and install version F0 1.11.3.

0693W00000WKMsrQAH.pngThanks and best regards,

"If you agree with my answer, please accept it by clicking on ""Accept as solution""."