Skip to main content
Roman
Associate II
Jun 6, 2019 2:35 PM UTC
Question

Steval-spin3201 hall sensors connection.

Hello!

I'm trying to work with steval-spin3201 board, i have AMETEC minijammer bldc motor with three hall sensors on board, ST Motor Control Workbench with Atolic True studio. First i tried sensor-less control and it's works fine with some tuning. But i can't rotate motor with hall sensors connected, motor stuck in one position and don't moving. What i did: in ST Motor workbench i selected Hall sensor instead of sensor-less, connected three hall sensor to board with 5V_USB power. I checked signal on hall sensors: it changes when motor rotating, so they alive. Can you suggest something? Thanks!

Some update: i managed to rotate motor with the hall sensors, i have to change "Sensors displacement" to 60 deg (because of hardware placement of sensors), but i can't understand what is "Placement electrical angle" mean?

Regards,

Roman.

This topic has been closed for replies.

3 replies

LCK
Visitor II
Aug 7, 2019 8:18 AM UTC

Dear Roman,

I encounter the same problem with you, may i know which software version you are using? According the STM Motor library V4.3, you need to manually set up hall sensor. Refer to manual below, page 89 onwards.

https://www.st.com/content/ccc/resource/technical/document/user_manual/5e/5e/d2/cb/07/35/45/a6/CD00298474.pdf/files/CD00298474.pdf/jcr:content/translations/en.CD00298474.pdf

Roman
RomanAuthor
Associate II
Aug 7, 2019 9:02 AM UTC

Yes, thank you! That was a decision for me

Laurent Ca...
Senior III
Jun 22, 2021 8:32 AM UTC

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards