Skip to main content
gary239955_stm1_stmicro
Associate
April 16, 2019
Question

STEVAL-SPIN3201

STEVAL-SPIN3201

I have a motor connected to this board and just cannot get it to run correctly.

I get the start up error or speed feedback error when running the motor.

I am running the motor in sensor less mode using the sample software (SDK5x - STEVAL-SPIN3201 - BullRunning.stmcx) with adjusted parameters.

I get the motor to startup (appears to be correct) but then when it reaches target rpm it the fails (most of the time with startup error)

I am using ST motor control Workbench, STM 32 Cube and IAR

Please can you assist with getting the motor to actually spin.

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards