Skip to main content
Visitor II
Apr 29, 2026 1:13 PM UTC
Question

STEVAL-PTOOL4A doesn't operate with potentiometer (only motor pilot could do )

I have STEVAL-PTOOL4A connected to drive 

- 12V sensored BLDC motor 

- 2 pair poles 

- 16k rpm 

I faced 2 problems 

- First motor doesn't operate with potentiometer when used alone without the workbench

- leds doesn't  light

(( THE SYSTEM POWERED BY 12VDC 10A))

1 reply

GMA
ST Technical Moderator
Apr 30, 2026 3:44 PM UTC

Hello @moh007,

Thank you for your problem report.
For the potentiometer feature, the mc_task.c file is missing a required function call.

/* Includes ------------------------------------------------------------------*/
...
#include "mc_polpulse.h"
#include "mc_app_hooks.h" /*** Add line ***/
#include "fixpmath.h"
...
**
 * @brief Initializes the whole motor control subsystem according to user
 * configuration and parameters.
 * @param pMCIList motor control interface data structure that will be
 * initialized.
 */
__weak void MCboot( MCI_Handle_t* pMCIList[NBR_OF_MOTORS] )
{
...
 FOC_Clear(M1); 
 MC_APP_BootHook(); /*** Add line ***/
 LL_TIM_ClearFlag_UPDATE(TIM3);

STEVAL-PTOOL4A LED_INFO and LED_ERROR are not managed by default in projects generated by MCDSK.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA