Skip to main content
Slee.3
Associate
Aug 28, 2020 1:23 AM UTC
Solved

STEVAL-ESC001V1 - Workbench example doesn't work

Hi! I am trying to control sensorless BLDC motor using STEVAL-ESC001V1.

I finished profiling my motor and working on the example on Workbench

(STEVAL-ESC001V1 electronic speed control 5.4.0).

I opened the example on the workbench and set the motor parameters (I didn't change the name of the project)

and fed PWM through other STM32 kit.

Here are my external inputs and PWM signals I am generating (PWM is 490Hz).

I can hear the beep sound continuously without PWM signal and the motor barely moves like 1 degree changes per deep.

When I feed PWM signal, the beep sound is gone and the motor didn't move at all. Literally doing nothing.

(I was changing the PWM width from 1060us to 1700us, Still nothing)

What can be wrong here?

I am just guessing this can be happened due to the gain of OPAMP because I am using the big motor not like small ones for drones. It is 300W 3000RPM 12V 10A(Nominal).

 @Power Management and Motor Control​ 

Regards,

Sangrae

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
Oct 20, 2020 3:33 PM UTC

Dear @Slee.3​ 

In the meantime, we published a patch to fix this code example (see https://community.st.com/s/question/0D53W00000HwV8RSAV).

Did you try it?

Best regards

Laurent Ca...

5 replies

Slee.3
Slee.3Author
Associate
Aug 28, 2020 1:25 AM UTC

Pictures are missing

Laurent Ca...
Senior III
Sep 24, 2020 8:23 AM UTC

Dear @Slee.3​ 

What do you mean by "Pictures are missing".

Best regards

Laurent Ca...

Laurent Ca...
Laurent Ca...Best answer
Senior III
Oct 20, 2020 3:33 PM UTC

Dear @Slee.3​ 

In the meantime, we published a patch to fix this code example (see https://community.st.com/s/question/0D53W00000HwV8RSAV).

Did you try it?

Best regards

Laurent Ca...

Laurent Ca...
Senior III
Nov 2, 2020 8:43 AM UTC

Dear @Slee.3​ 

As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.

If not, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...

Laurent Ca...
Senior III
Jun 22, 2021 4:59 AM UTC

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK). 

Best regards