Skip to main content
Kamil1
Associate II
December 3, 2018
Question

STEVAL-ESC001v1 - Motor profiler - profiling failed

Hello,

I have tried to use Motor Profiler with ESC001v1 and drone rc outrunner motor: 14n12p (7 pole pairs), 6s, 600kv

Connection via St-link and Uart was succesfull, firmware uploaded to the board ESC001v1, but motor profiling failed.

Where could be a problem? How can get more information than only "profile failed" ?

Thank you

Kamil

This topic has been closed for replies.

3 replies

ritesh
Associate II
February 19, 2020

Getting same error with

STEVAL-IPM15B + NUCLEO-F303RE + X-NUCLEO-IHM09M1 

Have you found any solution?

Kamil1
Kamil1Author
Associate II
May 14, 2020

unfortunatelly I haven't found any solution, absolutely no answer or help from ST...

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards